additional packages are needed to build Qt-X11-4.8.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

additional packages are needed to build Qt-X11-4.8.0

1,067 次查看
Yuri
NXP Employee
NXP Employee

It would be wonderful to include additional packages below to Freescale LTIB distro so that users can build Qt-X11-4.8.0.

 

1.< libXV and videoproto > package in the LTIB for XVideo support.

2. < libXinerama > package in the LTIB for Xinerama support.

3. < libXcursor > package  in the LTIB for Xcursor support.

4. < libXi > package in the LTIB for Xi support.

 

Otherwise, Qt GUI operation have a display problem on the i.MX53 SABRE.

标记 (2)
0 项奖励
回复
2 回复数

700 次查看
Yuri
NXP Employee
NXP Employee

In order to inform customers about the needed (additional) packages, when
building Qt-X11-4.8.0  

0 项奖励
回复

700 次查看
KrishnaPavan
Contributor II

Hi,

If you know/[ have tried ] to add pakages, then you can do it on your own, I guess?

0 项奖励
回复