Yocto(eMMC with uuu)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Yocto(eMMC with uuu)

跳至解决方案
1,759 次查看
ylmzhsn_
Contributor III

Hi NXP, 

I am getting this error while using uuu does anyone know the error? (ubuntu 18.04)

 

***************************************

~/imx-yocto-bsp/build/tmp/deploy/images/imx8mpevk$ ls
Image
Image--5.4-r0-imx8mpevk-20221114122125.bin
Image-imx8mpevk.bin
imx8mp-ab2--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-ab2.dtb
imx8mp-ab2-imx8mpevk.dtb
imx8mp-ddr4-evk--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-ddr4-evk.dtb
imx8mp-ddr4-evk-imx8mpevk.dtb
imx8mp-evk--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-basler--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-basler.dtb
imx8mp-evk-basler-imx8mpevk.dtb
imx8mp-evk-basler-isi0--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-basler-isi0.dtb
imx8mp-evk-basler-isi0-imx8mpevk.dtb
imx8mp-evk-basler-isi0-isi1--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-basler-isi0-isi1.dtb
imx8mp-evk-basler-isi0-isi1-imx8mpevk.dtb
imx8mp-evk-basler-mixed-isp-isi--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-basler-mixed-isp-isi.dtb
imx8mp-evk-basler-mixed-isp-isi-imx8mpevk.dtb
imx8mp-evk-basler-ov2775--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-basler-ov2775.dtb
imx8mp-evk-basler-ov2775-imx8mpevk.dtb
imx8mp-evk-basler-ov5640--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-basler-ov5640.dtb
imx8mp-evk-basler-ov5640-imx8mpevk.dtb
imx8mp-evk-dsp--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-dsp.dtb
imx8mp-evk-dsp-imx8mpevk.dtb
imx8mp-evk-dsp-lpa--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-dsp-lpa.dtb
imx8mp-evk-dsp-lpa-imx8mpevk.dtb
imx8mp-evk.dtb
imx8mp-evk-dual-basler--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-dual-basler.dtb
imx8mp-evk-dual-basler-imx8mpevk.dtb
imx8mp-evk-dual-ov2775--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-dual-ov2775.dtb
imx8mp-evk-dual-ov2775-imx8mpevk.dtb
imx8mp-evk-flexcan2--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-flexcan2.dtb
imx8mp-evk-flexcan2-imx8mpevk.dtb
imx8mp-evk-imx8mpevk.dtb
imx8mp-evk-inmate--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-inmate.dtb
imx8mp-evk-inmate-imx8mpevk.dtb
imx8mp-evk-it6263-lvds-dual-channel--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-it6263-lvds-dual-channel.dtb
imx8mp-evk-it6263-lvds-dual-channel-imx8mpevk.dtb
imx8mp-evk-jdi-wuxga-lvds-panel--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-jdi-wuxga-lvds-panel.dtb
imx8mp-evk-jdi-wuxga-lvds-panel-imx8mpevk.dtb
imx8mp-evk-ov2775--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-ov2775.dtb
imx8mp-evk-ov2775-imx8mpevk.dtb
imx8mp-evk-ov2775-ov5640--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-ov2775-ov5640.dtb
imx8mp-evk-ov2775-ov5640-imx8mpevk.dtb
imx8mp-evk-pcie-ep--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-pcie-ep.dtb
imx8mp-evk-pcie-ep-imx8mpevk.dtb
imx8mp-evk-rm67191--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-rm67191.dtb
imx8mp-evk-rm67191-imx8mpevk.dtb
imx8mp-evk-root--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-root.dtb
imx8mp-evk-root-imx8mpevk.dtb
imx8mp-evk-rpmsg--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-rpmsg.dtb
imx8mp-evk-rpmsg-imx8mpevk.dtb
imx8mp-evk-sof-wm8960--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-sof-wm8960.dtb
imx8mp-evk-sof-wm8960-imx8mpevk.dtb
imx8mp-evk-spdif-lb--5.4-r0-imx8mpevk-20221114122125.dtb
imx8mp-evk-spdif-lb.dtb
imx8mp-evk-spdif-lb-imx8mpevk.dtb
imx8mp_m7_TCM_hello_world.bin
imx8mp_m7_TCM_rpmsg_lite_pingpong_rtos_linux_remote.bin
imx8mp_m7_TCM_rpmsg_lite_str_echo_rtos.bin
imx8mp_m7_TCM_sai_low_power_audio.bin
imx-boot
imx-boot-imx8mpevk-sd.bin-flash_evk
imx-boot-tools
imx-image-full.env
imx-image-full-imx8mpevk-20221114122125.rootfs.manifest
imx-image-full-imx8mpevk-20221114122125.rootfs.tar.bz2
imx-image-full-imx8mpevk-20221114122125.rootfs.wic.bmap
imx-image-full-imx8mpevk-20221114122125.rootfs.wic.bz2
imx-image-full-imx8mpevk-20221114122125.testdata.json
imx-image-full-imx8mpevk.manifest
imx-image-full-imx8mpevk.tar.bz2
imx-image-full-imx8mpevk.testdata.json
imx-image-full-imx8mpevk.wic.bmap
imx-image-full-imx8mpevk.wic.bz2
imx-image-full-imx-imx-boot-bootpart.wks
lpddr4_pmu_train_1d_dmem_202006.bin
lpddr4_pmu_train_1d_imem_202006.bin
lpddr4_pmu_train_2d_dmem_202006.bin
lpddr4_pmu_train_2d_imem_202006.bin
modules--5.4-r0-imx8mpevk-20221114122125.tgz
modules-imx8mpevk.tgz
signed_dp_imx8m.bin
signed_hdmi_imx8m.bin
tee.bin
tee.mx8mpevk.bin
u-boot.bin
u-boot.bin-sd
u-boot-imx8mpevk.bin
u-boot-imx8mpevk.bin-sd
u-boot-sd-2020.04-r0.bin
u-boot-spl.bin
u-boot-spl.bin-imx8mpevk
u-boot-spl.bin-imx8mpevk-2020.04-r0-sd-2020.04-r0
u-boot-spl.bin-imx8mpevk-sd
u-boot-spl.bin-sd
uuu

*******************************

Boot Switch  0001 - of-of-of-on

uuu -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk imx-image-full-imx8mpevk.wic.bz2

 

Error : 

 

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Success 0 Failure 1


1:3 1/ 0 [Failure open usb device,Try sudo uuu ]

 

Best  Regards

Hasan Yılmaz

 

 

 

 

0 项奖励
回复
1 解答
1,742 次查看
ylmzhsn_
Contributor III

Hi Alejandro I found the error. 

 

sudo uuu -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk imx-image-full-imx8mpevk.wic.bz2

 

I was getting an error because I didn't add sudo. Thank you for the help

Best Regards Hasan Yılmaz

在原帖中查看解决方案

3 回复数
1,753 次查看
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @ylmzhsn_ 

Could you please try the command:

uuu -lsusb

 

And please send screenshot of the output.

Regards!

0 项奖励
回复
1,743 次查看
ylmzhsn_
Contributor III

Hi Alejandro I found the error. 

 

sudo uuu -b emmc_all imx-boot-imx8mpevk-sd.bin-flash_evk imx-image-full-imx8mpevk.wic.bz2

 

I was getting an error because I didn't add sudo. Thank you for the help

Best Regards Hasan Yılmaz

1,744 次查看
ylmzhsn_
Contributor III

imx-yocto-bsp/build/tmp/deploy/images/imx8mpevk$ uuu -lsusb
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion
==================================================
1:3 MX865 SDPS: 0x1FC9 0x0146 0x0002

 

0 项奖励
回复