Hi,
I'm using a Variscite's SoM based on i.MX6q. I'm trying to compile (from Yocto krogoth) the GPU drivers since JavaFX depend on this. But I'm getting not found error (HTTP 404). Can anybody confirm about this?
Here is the error: Vivante fetch error · GitHub
Regards,
Edit:
Browsing to http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/ gives me:
The system is currently unavailable.
Please accept our apologies for any inconvenience this may cause.
Feel free to contact our Technical Helpline at one of the following numbers:
Can anybody confirm? Anyway, I'll try again later.
Regards,
解決済! 解決策の投稿を見る。
Tested this as well, older versions are online, for example the 8.4:
http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-viv-5.0.11.p8.4-hfp.bin
If you don't provide a binary name, the website returns by default the "currently unavailable" message. So that's normal.
But we will check why the v8.6 is not there.
Regards,
Bernhard.
Hi.
Until this issue is fully resolved, Variscite has uploaded the missing files to their FTP server.
Please see the details here:
Unable to fetch Freescale/NXP binaries in Yocto Krogoth - Variscite Forums
Regards,
Eran
I discretely tested a few of these missing files and they can be found now on the server http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/...
So try building it again, hopefully it has been fully resolved.
Regards,
Bernhard.
Hello ---
I am trying to build the Yocto Morty version which is failing to fetch: imx-gpu-viv-5.0.11.p8.7-hfp.bin
Is there any workaround for this? Or are the files available elsewhere?
Thanks
Dear Mr. Fink,
since yesterday afternoon building works again.
Thank you and best regards
Ralf Spengler
Ralf Spengler
Softwareentwicklung
HEITEC AG
Werner-von-Siemens-Str. 61
91052 Erlangen
Telefon: 09131/877-180
Mobil: 0151/56036071
E-Mail: ralf.spengler@heitec.de<mailto:ralf.spengler@heitec.de>
Internet: www.heitec.de<http://www.heitec.de>;
Von: bernhardfink
Gesendet: Mittwoch, 14. Dezember 2016 13:25
An: Ralf Spengler
Betreff: Re: - Re: Yocto can't fetch imx-gpu-viv-5.0.11.p8.6-hfp.bin
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: Yocto can't fetch imx-gpu-viv-5.0.11.p8.6-hfp.bin
reply from Bernhard Fink<https://community.nxp.com/people/bernhardfink?et=watches.email.thread> in i.MX Community - View the full discussion<https://community.nxp.com/message/860383?commentID=860383&et=watches.email.thread#comment-860383>
Hi All,
There are also,too:
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-qtapplications-1.0.9.bin;fsl-eula=true
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-5.7.tar.gz
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-gst1.0-plugin-4.1.4.tar.gz
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-codec-4.1.4.bin;fsl-eula=true
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-sdk-2.3.2.bin;fsl-eula=true
I want to use Qt on my SABRSD(iMX6 Dual-Lite).
But I cannot do this , Because many packages cannot be downloaded like this.
Please give me some solution about this.
Regards.
Hi all,
Any updates?
There are many packages cannot be downloaded with L4.1.15_2.0.0_LINUX_DOCS release:
http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-viv-5.0.11.p8.6-hfp.bin
http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/kernel-module-imx-gpu-viv-5.0.11.p8.6.tar.gz
http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-lib-5.5.tar.gz
http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-vpu-5.4.35.bin
....
Regards
Tested this as well, older versions are online, for example the 8.4:
http://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-viv-5.0.11.p8.4-hfp.bin
If you don't provide a binary name, the website returns by default the "currently unavailable" message. So that's normal.
But we will check why the v8.6 is not there.
Regards,
Bernhard.
Hi Bernhard,
Have you got more information about that problem?
Regards
Darek
I'm evaluating an i.MX6-based hardware-module for a customer, but currently, because of the missing files, there's not much I can do since monday. Is there a timeline when the following resources will be available again?
If they do not become available soon again, I'm afraid I have to recommend not to use an i.MX6-based hardware (or hardware depending on NXP-products generally) because of a lack of support. It should be possible to bring these files up again within a few days.
Any chance this get resolved soon ?
Hi Bernhard,
Thanks for your reply,
I'm attaching some more information:
The layer is meta-fsl-bsp-release:
[geckos@csi24 meta-fsl-bsp-release]$ git log -1
commit 90399d99af8a2660ebe50b49752e95b210239fd9
Author: Jun Zhu <junzhu@nxp.com>
Date: Fri Nov 4 17:22:41 2016 +0800
linux-imx: Add 2 audio patches
- 0001-MLK-13418-ASoC-wm8960-workaround-no-sound-issue-in-m.patch (updated)
- 0002-MLK-13422-ASoC-wm8960-fix-the-pitch-shift-issue-afte.patch (new added)
Signed-off-by: Jun Zhu <junzhu@nxp.com>
[geckos@csi24 meta-fsl-bsp-release]$ git remote -v show
fsl-release git://git.freescale.com/imx/meta-fsl-bsp-release (fetch)
fsl-release git://git.freescale.com/imx/meta-fsl-bsp-release (push)
The version is preferred by fsl-imx-preferred-env.inc:
[geckos@csi24 meta-fsl-bsp-release]$ grep -R --include "*.inc" 8.6 .
./imx/meta-sdk/conf/distro/include/fsl-imx-preferred-env.inc:PREFERRED_VERSION_imx-gpu-viv_mx6 = "5.0.11.p8.6-hfp"
./imx/meta-sdk/conf/distro/include/fsl-imx-preferred-env.inc:PREFERRED_VERSION_xf86-video-imxfb-vivante_mx6 = "5.0.11.p8.6"
./imx/meta-sdk/conf/distro/include/fsl-imx-preferred-env.inc:PREFERRED_VERSION_kernel-module-imx-gpu-viv_mx6 = "5.0.11.p8.6"
Which is included by this distro files:
[geckos@csi24 meta-fsl-bsp-release]$ grep -R --include "*.conf" fsl-imx-preferred-env.inc .
./imx/meta-sdk/conf/distro/fsl-imx-fb.conf:include conf/distro/include/fsl-imx-preferred-env.inc
./imx/meta-sdk/conf/distro/fsl-imx-wayland.conf:include conf/distro/include/fsl-imx-preferred-env.inc
./imx/meta-sdk/conf/distro/fsl-imx-x11.conf:include conf/distro/include/fsl-imx-preferred-env.inc
./imx/meta-sdk/conf/distro/fsl-imx-xwayland.conf:include conf/distro/include/fsl-imx-preferred-env.inc
Thanks to your advice I could circunvent the problem by using this patch: meta-fsl-bsp-release change version of imx-gpu-viv from 8.6 to 8.4 · GitHub
I'll keep using this by now. I didn't had the chance to boot up a image yet. At any problem I came back here :smileyhappy:
Regards and thanks!