Why is the image generated by the Android 12.0.0_1.0.0 BSP using Linux version 5.10.66?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why is the image generated by the Android 12.0.0_1.0.0 BSP using Linux version 5.10.66?

579 次查看
ChChang
Contributor II

Hi

I downloaded the Android 12.0.0_1.0.0 BSP and generated the image according to the user guide.

As per the instructions, the Linux kernel version should be 5.10.72, but after flashing it to the i.MX8MP-EVK, the Linux kernel version is 5.10.66.

I have already checked the contents of the Makefile and utsrelease.h, and both show 5.10.72. How can I configure the image to use Linux kernel version 5.10.72?


0 项奖励
回复
1 回复

550 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, the android 12 comes with several error in building is better to download the Android 12.1.0_1.0.0 (L5.15.52_2.1.0 BSP)

 

Regards

0 项奖励
回复