Why exactly did NXP suddenly disable PCIe Advanced Error Reporting (AER) in their latest Linux BSP LF5.15.52_2.1.0 (Sep 2022)? So far in previous BSPs you guys had this always enabled. Is there any issue with using it? Thanks!
So NXP is unable to answer our questions?
NXP dares to shed some light on this topic?
LF5.15.52 didn't disable PCIE AER
NXP dares to share what is going on here?
I still not get the update from our expert, for the adding question you can use "pcie_ports=native"
Please refer to our newest released, details reason I will help confirm.
Hi,
any news about it?
Another question:
CONFIG_PCIEAER and CONFIG_PCIEAER_INJECT can be used for a production kernel?
I must also use "pcie_ports=native" as kernel parameter or it is unnecessary?
Thanks,
Flavio