Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which RPA version to use for i.MX 8QXP-C0 rev. using SCFW version 1.9.0 for MT53D1024M32D4DT ?

Jump to solution
3,217 Views
r_trivedi123
Contributor IV

Hi,
I am worrking on a custom hardware having i.mx8qxp-c0 revision cpu.

I am using LF5.10.35_2.0.0 from here.

As per this guide i have downloaded scfw-kit-1.9.0.

I have used MT53D1024M32D4DT-053 AAT:D LPDDR4 micro.

I have been through the link provided.

My query is which RPA tool will be aligned with scfw-kit-1.9.0. and LF5.10.35_2.0.0 ?

Also I am not able to find LPDDR's parameters(Density per channel , total DRAM density, total number of CS used etc.) or datasheet from micron technology, so how do i proceed ?

Any help would be appreciated.

--
Thanks
Rutvij

 

 

Tags (4)
0 Kudos
Reply
1 Solution
3,192 Views
igorpadykov
NXP Employee
NXP Employee

yes for i.MX8QXP LPDDR4 it is v.16.

 

Best regards
igor

 

 

View solution in original post

0 Kudos
Reply
3 Replies
3,195 Views
r_trivedi123
Contributor IV

Hi Igor,
Thanks for the quick replay.

The suggested link has versions 15,16,21 available(image attached), will version 16 be good to go with?

--
Thanks




0 Kudos
Reply
3,193 Views
igorpadykov
NXP Employee
NXP Employee

yes for i.MX8QXP LPDDR4 it is v.16.

 

Best regards
igor

 

 

0 Kudos
Reply
3,199 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rutvij

 

one can use latest version from link

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-DXP-DX-DDR-Register-Programming...

 

Best regards
igor

0 Kudos
Reply