Which PCB material is the best? in i.mx9352

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which PCB material is the best? in i.mx9352

558 Views
vivek5676
Contributor II

Hi,

Please advice Which PCB material is the best? in i.mx9352.

Regards,

Vivek Kumar

0 Kudos
Reply
2 Replies

523 Views
vivek5676
Contributor II

Thanks !

0 Kudos
Reply

531 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the user guide, PCB material: the material used on EVK is 185HR.

for other material select, pls refer to this

Material characteristics such as the Coefficient of Thermal Expansion (CTE) should be considered. The CTE describes how a material changes dimension with temperature. Ideally, a PCB material’s CTE should be closely matched to copper, which is about 17 ppm°C. CTE is a concern because as the PCB expands during heating, it can elongate plated via holes and cause fracturing.
If the CTE is closely matched to copper, expansion of the PCB material and copper will be more uniform and the plated via holes will be more robust during thermal cycling.

0 Kudos
Reply