Which LVDS displays fit to SABRE board with i.MX6QP (Quad Plus (!), MCIMX6QP-SDB)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which LVDS displays fit to SABRE board with i.MX6QP (Quad Plus (!), MCIMX6QP-SDB)?

1,441 次查看
martin_maurer
Contributor III

Does someone know which LVDS display(s) can be connected

to SABRE board with i.MX6QP (Quad Plus (!), MCIMX6QP-SDB)?

What cables are needed to connect this display?

As far as I know there are both LVDS connectors on this board.

Same display and cable can be used on both ports.

Is the active usage of two LVDS displays possible (different pictures) at the same time?

Even different size, frequency and resolution possible

or is there something which is not independent?

标签 (2)
0 项奖励
4 回复数

812 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

HannStar lcd is used with boards

IPU Usage on IMX6 processor..

for other driver customization may be needed, useful examples

can be found on

https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/

https://community.freescale.com/thread/373763

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励

812 次查看
martin_maurer
Contributor III

Many thanks for your answer!

So I can order

1x MCIMX6QP-SDB

2x MCIMX-LVDS

and they fit together (at least from hardware point of view)?

All needed (LVDS) cables to connect it to IMX6 board are already delivered with the LVDS displays?

And they are long enough to connect both at the same time?

Or must I order something separately?

0 项奖励

812 次查看
igorpadykov
NXP Employee
NXP Employee

right, these are correct part numbers.

~igor

0 项奖励

812 次查看
vageeshpanditha
Contributor II

Dear Igor,

Please confirm whether MCIMX-LVDS1 works with MCIMX6QP-SDB and whether MCIMX-LVDS and MCIMX-LVDS1 is same or different.

Regards,

Vageesh K M

Arrow, India

0 项奖励