Which LVDS displays fit to SABRE board with i.MX6QP (Quad Plus (!), MCIMX6QP-SDB)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which LVDS displays fit to SABRE board with i.MX6QP (Quad Plus (!), MCIMX6QP-SDB)?

1,370 Views
martin_maurer
Contributor III

Does someone know which LVDS display(s) can be connected

to SABRE board with i.MX6QP (Quad Plus (!), MCIMX6QP-SDB)?

What cables are needed to connect this display?

As far as I know there are both LVDS connectors on this board.

Same display and cable can be used on both ports.

Is the active usage of two LVDS displays possible (different pictures) at the same time?

Even different size, frequency and resolution possible

or is there something which is not independent?

Labels (2)
0 Kudos
4 Replies

741 Views
igorpadykov
NXP Employee
NXP Employee

Hi Martin

HannStar lcd is used with boards

IPU Usage on IMX6 processor..

for other driver customization may be needed, useful examples

can be found on

https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/

https://community.freescale.com/thread/373763

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

741 Views
martin_maurer
Contributor III

Many thanks for your answer!

So I can order

1x MCIMX6QP-SDB

2x MCIMX-LVDS

and they fit together (at least from hardware point of view)?

All needed (LVDS) cables to connect it to IMX6 board are already delivered with the LVDS displays?

And they are long enough to connect both at the same time?

Or must I order something separately?

0 Kudos

741 Views
igorpadykov
NXP Employee
NXP Employee

right, these are correct part numbers.

~igor

0 Kudos

741 Views
vageeshpanditha
Contributor II

Dear Igor,

Please confirm whether MCIMX-LVDS1 works with MCIMX6QP-SDB and whether MCIMX-LVDS and MCIMX-LVDS1 is same or different.

Regards,

Vageesh K M

Arrow, India

0 Kudos