Does someone know which LVDS display(s) can be connected
to SABRE board with i.MX6QP (Quad Plus (!), MCIMX6QP-SDB)?
What cables are needed to connect this display?
As far as I know there are both LVDS connectors on this board.
Same display and cable can be used on both ports.
Is the active usage of two LVDS displays possible (different pictures) at the same time?
Even different size, frequency and resolution possible
or is there something which is not independent?
Hi Martin
HannStar lcd is used with boards
for other driver customization may be needed, useful examples
can be found on
https://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/
https://community.freescale.com/thread/373763
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Many thanks for your answer!
So I can order
1x MCIMX6QP-SDB
2x MCIMX-LVDS
and they fit together (at least from hardware point of view)?
All needed (LVDS) cables to connect it to IMX6 board are already delivered with the LVDS displays?
And they are long enough to connect both at the same time?
Or must I order something separately?
right, these are correct part numbers.
~igor
Dear Igor,
Please confirm whether MCIMX-LVDS1 works with MCIMX6QP-SDB and whether MCIMX-LVDS and MCIMX-LVDS1 is same or different.
Regards,
Vageesh K M
Arrow, India