Hi all Please tell me the place of the document. In P7 of Freescale Yocto Project User's Guide (Rev L3.10.17_1.0.0-ga), there is a description as below. However, I can not find it from community and Freescale Web site. "For more information on Uboot configuration, see the Freescale U-Boot User’s Guide." Please tell me !! Best Regards,
已解决! 转到解答。
Hi ko-hey
please refer to attached document Chapter 1.
All released documents are included in Doc bundle:
L3.10.17_1.0.0_LINUX_DOCS Linux 3.10.17 BSP & MM Bundle
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ko-hey
please refer to attached document Chapter 1.
All released documents are included in Doc bundle:
L3.10.17_1.0.0_LINUX_DOCS Linux 3.10.17 BSP & MM Bundle
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor
Thank you for quick reply.
Do you mean that there is a no document that is named "Freescale U-Boot User's Guide” ?
Were the document integrated to "Freescale Yocto Project User's Guide” ?
Best Regards,
ko-hey