Morning NXP world.
I need some help. I have one very old IMX8M Mini EVK board. board version is "SCH-31407 REV A" . PCB board color is black , not Green, and boot switch is 8 pin only , not 10 pin.
Where can I find yocto BSP image and boot switch setting suitable for this version of EVK ? I try to use yocto bsp version 'L4.14.98_2.0.0_ga_images_MX8MMEVK' and I can not boot on.
Thank you.
Leo
Hi leolarrel@gmail.com,
You can find the boot mode settings on the board itself. They have given the boot mode settings table on the board.
For the images concern, all the supported Linux BSP for i.MX8M Mini EVK can be run on the board (black as well as green). You can find the Linux BSP and its documents from this link.
Hope this will help you.
If you still face any issue, please let us know.
Regards,
Shivani