Where can I download patches for Android 5.0 (Lollipop)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I download patches for Android 5.0 (Lollipop)?

ソリューションへジャンプ
3,369件の閲覧回数
GregDyess
Contributor III

Where can I download the necessary patches and code for Android 5.0 (Lollipop) for i.MX6?  I read an article indicating Freescale had this running already.

ラベル(8)
1 解決策
1,550件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gregory

it is preliminary release not publicly available, but

you can ask local FAE to obtain it from internal site.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,551件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gregory

it is preliminary release not publicly available, but

you can ask local FAE to obtain it from internal site.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,550件の閲覧回数
gavinbao
Contributor I

Where can I download the Android 5.0 (Lollipop) for i.MX6? Please tell me .Thanks.

0 件の賞賛
返信
1,550件の閲覧回数
GregDyess
Contributor III

Thanks for the information.  Since it is not ready for release, I'll hold off trying to use it for a client's board.

Any idea when it might be released publicly?

0 件の賞賛
返信
1,550件の閲覧回数
ddejean
Contributor II

Hi Gregory,

I already contacted FAE for the same (almost) question and Alfredo from Freescale Technical support answered me (I quote) :

Our developers team almost release the android L5.0.0 based on 5.0.0_r6 which include kernel 3.10.53 and latest vivante binaries 5.0.11p4 the release in schedule to appears public on December 29th on the Freescale website

The sources are still not available on the mentionned website but according to the previous message I assume  it should come quickly. If anyone can confirm that, it would be great :smileyhappy:

Best regards

1,550件の閲覧回数
GregDyess
Contributor III

Any update on this?

0 件の賞賛
返信