Dear All,
I have a question about Gated Clock Mode in i.MX6DQ.
Refer to attached file.
Is it possible to input data right in Period 1 and Period 2?
Period 1 : 41508 pixclk (=1650pixel x 25line + 258pixel)
Period 2 : 8362 pixclk (=1650pixel x 5line + 112pixel)
[Condition]
- pixclk frequency : 74.25MHz
- Total Line count / frame (Blanking Line + Active Line) : 750
- Active Line count / frame (hsync count) : 720
- Total pixclk count / line (Included blanking) : 1650
- Active pixclk count / line : 1280
Best Regards,
Keita
解決済! 解決策の投稿を見る。
As per the diagram you've provided, the Period 1 overlaps the first active pclk clock, i.e. the first pclk clock when Vsync is active. So, at this moment, data is captured. Also, the Period 2 overlaps the last active pclk clock, i.e. the last pclk clock when Vsync is active. So, at this moment, data is captured as well.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
In the Gated Clock mode, when the Hsync signal is inactive (low), no data capture is possible. Data is captured only when Hsync is active (high).
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Autur,
Hello. Thank you for your reply.
>In the Gated Clock mode, when the Hsync signal is inactive (low), no data capture is possible.
>Data is captured only when Hsync is active (high).
Yes. We have already known above thing.
Refer to attached file again.
Is it possible to input data right with Period 1 and Period 2?
(Please consider the Period 1 and Period 2)
Best Regards,
Keita
As per the diagram you've provided, the Period 1 overlaps the first active pclk clock, i.e. the first pclk clock when Vsync is active. So, at this moment, data is captured. Also, the Period 2 overlaps the last active pclk clock, i.e. the last pclk clock when Vsync is active. So, at this moment, data is captured as well.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Artur,
Thank you for your reply.
>i.e. the first pclk clock when Vsync is active
Is your meaning Hsync is active?
Do you find another problem?
Best Regards,
Keita
Oh, sorry. Of course, I meant Hsync in both cases.
Best Regards,
Artur
Hi Artur,
OK. Thank you very much!
Best Regards,
Keita