Hi ALL,
I want to use L3.14.28_1.0.0 bsp. But I can't find where download L3.14.28_1.0.0 source. Who can help me ?
Thanks!
已解决! 转到解答。
Hi Shannon
please check FSL BSP
L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo
Linux Binary Demo Files and Linux BSP Documentation
or Community
meta-fsl-arm - Layer containing Freescale ARM hardware support metadata
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
I checked, but available version of Linux is 3.10.17.
See below logs. Only available version is 3.10.17 from 3.14.28BSP
Please let me know if I missed some procedure!
bitbake core-image-minimal
Parsing recipes: 100% |###########################################| Time: 00:01:51
Parsing of 1581 .bb files complete (0 cached, 1581 parsed). 2051 targets, 127 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
NOTE: preferred version 3.14.28-1.0.0 of linux-imx not available (for item virtual/kernel)
NOTE: versions of linux-imx available: 3.10.17
NOTE: preferred version 3.14.28-1.0.0 of linux-imx not available (for item kernel-base)
NOTE: versions of linux-imx available: 3.10.17
NOTE: preferred version 3.14.28-1.0.0 of linux-imx not available (for item kernel-image)
NOTE: versions of linux-imx available: 3.10.17
Hi Shannon
please check FSL BSP
L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo
Linux Binary Demo Files and Linux BSP Documentation
or Community
meta-fsl-arm - Layer containing Freescale ARM hardware support metadata
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
In the L3.14.28_1.0.0_iMX6QDLS_BUNDLE there are two tar pkgs.(fsl-yocto-3.14.28-1.0.0.tar.gz and L3.14.28_1.0.0_ga_images_MX6.tar.gz)
But fsl-yocto-3.14.28-1.0.0.tar.gz is doc.
L3.14.28_1.0.0_ga_images_MX6.tar.gz is images.
Don't have bsp source in L3.14.28_1.0.0_iMX6QDLS_BUNDL.
Best regards
Shannon