Where can I download L3.14.28_1.0.0 bsp source?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I download L3.14.28_1.0.0 bsp source?

Jump to solution
2,732 Views
guohn
Contributor III

Hi ALL,

     I want to use L3.14.28_1.0.0 bsp. But I can't find where download L3.14.28_1.0.0 source. Who can help me ?

Thanks!

Labels (1)
0 Kudos
1 Solution
1,679 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shannon

please check FSL BSP

L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo

Linux Binary Demo Files and Linux BSP Documentation

or Community

meta-fsl-arm - Layer containing Freescale ARM hardware support metadata

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
9 Replies
1,679 Views
jiyoonchung
Contributor I

I found 3.14.28 from L3.14.28-1.0.1.patch

Thanks

James

0 Kudos
1,679 Views
jiyoonchung
Contributor I

Hi

I checked, but available version of Linux is 3.10.17.

See below logs. Only available version is 3.10.17 from 3.14.28BSP

Please let me know if I missed some procedure!

bitbake core-image-minimal
Parsing recipes: 100% |###########################################| Time: 00:01:51
Parsing of 1581 .bb files complete (0 cached, 1581 parsed). 2051 targets, 127 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
NOTE: preferred version 3.14.28-1.0.0 of linux-imx not available (for item virtual/kernel)
NOTE: versions of linux-imx available: 3.10.17
NOTE: preferred version 3.14.28-1.0.0 of linux-imx not available (for item kernel-base)
NOTE: versions of linux-imx available: 3.10.17
NOTE: preferred version 3.14.28-1.0.0 of linux-imx not available (for item kernel-image)
NOTE: versions of linux-imx available: 3.10.17

0 Kudos
1,679 Views
Yuri
NXP Employee
NXP Employee

   Please follow recommendations of "Freescale_Yocto_Project_User's_Guide.pdf"

in documentation package. The sources are loaded from git during building.

Regards,

Yuri.

1,679 Views
jiyoonchung
Contributor I

Hi

I did, but I found that Linux-imx was version 3.10.17.

I changed PREFERRED_VERSION, but no luck.

Yuri, did you try?

Thanks

James

0 Kudos
1,679 Views
Yuri
NXP Employee
NXP Employee

  Hope the following helps.

“how can i get imx-3.14.28-1.0.0_ga”

https://community.freescale.com/message/510218#510218

Regards,
Yuri.

0 Kudos
1,679 Views
guohn
Contributor III

OK, Thanks ALL

0 Kudos
1,680 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shannon

please check FSL BSP

L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo

Linux Binary Demo Files and Linux BSP Documentation

or Community

meta-fsl-arm - Layer containing Freescale ARM hardware support metadata

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,679 Views
guohn
Contributor III

Hi igor,

     In the L3.14.28_1.0.0_iMX6QDLS_BUNDLE there are two tar pkgs.(fsl-yocto-3.14.28-1.0.0.tar.gz and L3.14.28_1.0.0_ga_images_MX6.tar.gz)

     But fsl-yocto-3.14.28-1.0.0.tar.gz is doc.

     L3.14.28_1.0.0_ga_images_MX6.tar.gz is images.

     Don't have bsp source in L3.14.28_1.0.0_iMX6QDLS_BUNDL.

Best regards

Shannon

0 Kudos
1,679 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shannon


please read document Freescale_Yocto_Project_User's_Guide.pdf

it shows how to obtain sources.


~igor

0 Kudos