Is it possible to run weston as a non-root-user? Or run weston as root-user and start applications as non-root-user?
Currently weston is running with drm-backend as root user, starting as systemd-service.
Once weston is started I can see a desktop-shell on my screen. Then I can start a simple qt-application as root-user. But I can't start that qt-application as non-root-user because the application failed to create wl_display (Permission denied).
I figgured out that it has someting to do with the owner of wayland-0.lock. If I change the owner of wayland-0 to the non-root-user I was able to start the qt-application.
But step-by-step
1. XDG_RUNTIME_DIR variable:
For wayland/weston it is neccessary to set the environment variable XDG_RUNTIME_DIR to a folder. This folder should have the permissions 0700. This environment variable is set in a shell script called weston.sh in /etc/profile.d/. In my understanding this script is only called when a user login, isn't it.
On the other hand the service manager has its own environment. That means that the XDG_RUNTIME_DIR variable should set in the service by Environmet= or by EnvironmentFile=.
2. weston-start
I disabled the weston.service by removing it from /lib/systemd/system/ and tried to start weston manually as non-root-user by the weston-start script. In main the script sets the XDG_RUNTIME_DIR variable and call openvt with weston-launch as command. I got the error message "Couldn't get a file descriptor referring to the console". Openvt creates a new virtual console where weston can assign to. My investigations showed that I only can call openvt as root-user. For example (as non-root-user logged in) sudo openvt weston-start. But in this case weston starts as root again and I am not able to start a qt-application as (non-root-user).
Is it possible to start weston on a i.MX 8MP as non-root-user?
In my opinion not becaus the backend (drm-backend) and openvt needs root access.
Is it possible to start weston as root-user and run qt-applications non-root-user?
I think no because wayland-0.lock belongs to the root-user und because of that a non-root-user can have access to it.
Is there a way maybe to start weston as root-user and enable non-root-user to communicate with the display-server?
Thanks