Wandboard DL SD card readiness

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wandboard DL SD card readiness

942件の閲覧回数
lyfsci
Contributor III

Hi Experts,

I am not able to find procedure for flashing the Android 5.0.1 build into the SD card for Wandboard DL. I am able to successfully compile the repository and the images are generated. It would be great if I could be pointed to few documentation regarding the same.

I tried flashing using the fsl script where it expects "u-boot.imx" file which is not generated as part of compilation.

Regards,

Lyf

ラベル(3)
0 件の賞賛
返信
1 返信

864件の閲覧回数
art
NXP Employee
NXP Employee

Refer to attached Quick Start Guide document (starting from the Page 2). This document is also available on the Wandboard web site:

http://www.wandboard.org/index.php/downloads


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信