Hi,
I am testing video in i.MX6 DL boards with playwnd and windows video player in WEC 7.
In some i.MX6 DL boards video is playing but hanging after some time. In other it is not at all working.
I am getting "waiting for VPU interrupt at frame 0 " and "VPU busy and hung" prints, Player will hang if I try to close it.
What could be the reason for this issue? How can I solve this issue ?
Can anyone help me on this issue ? Thanks in advance.
With regards,
Kavya D.C
Have you try the same with Linux? It would be good to add the video that you are using for testing.
Deactivated user, Can you please comment
Ya i tried Linux on the same boards, Videos are working fine.
Any changes are required in i.MX6DL boards with respect to VPU or multimedia libraries ?
Hello KavyaDC,
If Linux it is working fine, this means that the VPU libraries it is not the problem it is something related with the integration with Windows, so let me ask again to Deactivated user, if they can help, since we are not WEC7 experts.
Best Regards
Jaime