Hi!
I’d like flash u-boot and the corresponding u-boot-environment image with UUU in the boot0 hardware partition of the eMMC storage of a Verdin iMX8MP SoM.
As per Toradex documentation I need to write the environment at offset 0x2200 (8704 bytes) before the end of boot0. The boot0 hardware partition of this eMMC has size 32MiB.
For this reason I created a complete image with the size of the boot0.
The image is created using dd and appending the imx-boot image, zeros until the U-Boot environment image.
|-imx-boot-|------------|--env---|
| | zeros | |
|----------|------------|--------|
0x0 -0x2200 END
I'm trying to flash this image into the bootloader partition using the script below.
uuu_version 1.4.127
...
...
FB: ucmd setenv fastboot_dev mmc
FB: flash bootloader my_bootloader
FB: ucmd setenv mmcdev 2
FB: flash -raw2sparse all my_image.wic
FB: done
I can enter correctly in Fastboot mode but I always get the following error message:
0x40000000image too large for partition1:214>Fail image too large for partition(1.089s)
Looking at the fastboot code in U-Boot it looks like “FB: flash bootloader” does not support writing more than 4MiB.
Is there any way to perform one or more of the following using UUU?
- write more than 4MiB on a boot0 hardware partition?
- write at a specified offset on a boot0 hardware partition?
Thanks!