Use SPI on imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use SPI on imx6q

754件の閲覧回数
levanthuan
Contributor I

I want to use spi for tranmit data path SPI1 SS0, Can I using function on uboot? Help me! Thank!

ラベル(1)
0 件の賞賛
返信
1 返信

563件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi,

     I checked the i.MX6Q SabreSD board, there is a SPI NOR flash connected to CSPI1_SS0, so you can try using 'sf' command in uboot to write/read data on this SPI NOR flash, please see the help in uboot about 'sf' command and try it, thanks.

0 件の賞賛
返信