Unused DQ pins of i.MX6S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unused DQ pins of i.MX6S

Jump to solution
1,180 Views
torus1000
Contributor V

Hi all,

I believe i.MX6S and i.MX6DL has same pins but i.MX6S only supports 32b DDR3.

Is it OK to leave unused DQ pins open?

Thanks.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
986 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes it is OK. In general it may be useful to look at

AN4397  Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
987 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes it is OK. In general it may be useful to look at

AN4397  Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply