Hi
I am using the imx-android-13.4.1 code. after burn to my board ,It will suddenly
give the Unable to handle kernel paging request at virtual address error then crash. : (
Here is the information:
active wake lock PowerManagerService
request_suspend_state: wakeup (3->0) at 178405733691 (2013-07-09 10:09:59.364397999 UTC)
PHY: 1:05 - Link is Up - 1000/Full
mmc0: Starting deferred resume
mmc0: Deferred resume completed
Unable to handle kernel paging request at virtual address 9fed28f0
pgd = c0004000
[9fed28f0] *pgd=00000000
Internal error: Oops: 805 [#1] PREEMPT SMP
Modules linked in:
CPU: 1 Not tainted (3.0.35-05524-g8513494-dirty #5)
Any advice will be appreciate .
Thanks
已解决! 转到解答。
It is like that it is about the temperature after let the IMX6Q cool this problem like have solved . : )