Unable to build rtos application with Android Automotive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to build rtos application with Android Automotive

ソリューションへジャンプ
2,717件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

Unable to build hello world application for Android 9 Automotive got following error,

Configure hellow world in device-fsl. While building I got following error,

 

make[1]: *** No rule to make target 'm4_image.bin', needed by 'flash_all_spl_container_ddr_car'. Stop.

 

 

 

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
1 解決策
2,674件の閲覧回数
vinothkumars
Senior Contributor IV

I able to build standalone application by modifying the device-fsl.

Regards,
Vinothkumar Sekar

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,675件の閲覧回数
vinothkumars
Senior Contributor IV

I able to build standalone application by modifying the device-fsl.

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
2,695件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

to build an M4 rtos application you may do it using GCC Arm or IAR.

When compiled using any of these two toolchains you may use the M4 binary to create the flash.bin

Best regards,
Aldo.

0 件の賞賛
返信