Greetings
I am willing to interface a BT and WiFi module that is outputting 1.8V IO. Does this mean I have to use a 1.8/3.3V level converter for the interface of
UART and SDIO? Where exactly can I find the information regarding the voltage levels of different blocks say HDMI, SPI, I2S etc.
Regards,
Mete
解決済! 解決策の投稿を見る。
Hi Mete
voltage levels of different blocks (modules) are given in Table 22. GPIO I/O DC Parameters
i.MX6DQ Datasheet (rev.4, 7/2015) http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
where OVDD (block power supply) is given in Table 100. 21 x 21 mm Functional Contact Assignments
as "Power Group".
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Mete
voltage levels of different blocks (modules) are given in Table 22. GPIO I/O DC Parameters
i.MX6DQ Datasheet (rev.4, 7/2015) http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
where OVDD (block power supply) is given in Table 100. 21 x 21 mm Functional Contact Assignments
as "Power Group".
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
So if I supply the NVCC_EIM/NVCC_CSI which are the power rails for UART default pins, with GEN_1V8 frpm PF0100, then I won't be needing a level converter between a 1.8V I/O device and i.MX6Q for UART interfacing. Is this correct?
Thanks,
Mete
Hi Mete
correct
Best regards
igor