Hi Igor,
Yes, I could try this, thanks. But I have no such cable / adapter right now.
My custom board has 2 dedicated USB connectors for the USB_OTG2 port. One for host (type A) and one for device (type B). So it should be
no problem to test this functionality on this board.
But again, a basic test for the host functionality (USB key connected) already fails when dr_mode = "host" is configured in the device-tree. Both on
the custom board with mainline Linux and on the 14x-14 evk on mainline and imx_3.14.38_6ul_ga. At least in my current tests the USB key is
not detected with this dr_mode change any more. And if this does not work, testing the USB device (gadget) functionality does not yet make
much sense to me. I really would like to first see USB host still working in this OTG setup.
Could you perhaps test this on the 14x14 EVK and let me know, if this works for you?
Thanks,
Stefan