I installed an SPI flash device on the iMX6-smart-devices board and have a working interface to that.
I am currently booting/rebooting my board over USB using the imx_usb tool. Now I want to transition
a usb-based boot to SPI-boot. First, I have to reconfigure the BT_CFGX bits, and then it appears to me
that I can use the exact same image I boot over USB as the boot image for SPI-flash, true?
Solved! Go to Solution.
The important thing needed during boot from a storage media s to ensure that the bootloader has an Image Vector Table (IVT), this is used by ROM during Boot from a storage media.
If your image is downloaded using the imx_usb tool and has a an IVT, then the same image might work.
The reason I say might is because the IVT might not get exercised in Serial downloader mode (USB download). So you might see problems if the IVT is faulty when booting from SPI-NOR.
Adding text to my question, which explains why we are not able to boot from SPI
NOR Flash. This experiment uses the iMX6-SABRE Smart Devices Board.
The SPI Flash device (U14 on the schematic) is not populated. We populated the
device and I was able to interface with it at runtime (so that I could load it up with a
boot image).
The next step was to reconfigure the BOOT DIP switch and BT_CFG4 pins to use this
device as the boot device. This is where the trouble started. After a day of not seeing
the signals I expected to see (at boottime) on the device, we realized that the ROM
bootloader has the IOMUX configuration to use a different set of pins for ECSPI-1 boot
(refer to table 8-25 of reference manual).
Despite this problem, my question still holds: is the image format for a serial boot over USB
the same as the image that would be stored in a SPI-boot device?
For anyone looking for some empirical data on this, I can confirm that when booting off ECSPI5 on the smart devices board, I was able to use the exact same u-boot.bin file for booting off SD, USB or SPI-NOR.
The important thing needed during boot from a storage media s to ensure that the bootloader has an Image Vector Table (IVT), this is used by ROM during Boot from a storage media.
If your image is downloaded using the imx_usb tool and has a an IVT, then the same image might work.
The reason I say might is because the IVT might not get exercised in Serial downloader mode (USB download). So you might see problems if the IVT is faulty when booting from SPI-NOR.
Ok, thanks. I guess I'll just have to wait till I have hardware that allows me to prove it in.