Trouble booting from eMMC while updating i.mx6ul board from 2015 uboot.imx to 2017 SPL+uboot.img

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trouble booting from eMMC while updating i.mx6ul board from 2015 uboot.imx to 2017 SPL+uboot.img

1,667 Views
robertcagle
Contributor I

I am trying to update a custom imx6ul board from the NXP bsp u-boot
to the Community bsp u-boot.  The custom board boots from emmc okay using a 2015
NXP u-boot.imx image, but fails to boot from emmc with a 2017.11 or 2019.4 fslc
spl image. However, I am able to run the spl image if I manually load
it using usb-sdp or jtag.

I've tried:

a) checking imx_usb_loader scripts to make sure installation was done correctly.
    dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=512 conv=fsync count=8
    echo 0 > /sys/block/mmcblk1boot0/force_ro
    dd if=SPL of=/dev/mmcblk1boot0 bs=512 seek=2
    dd if=u-boot.img of=/dev/mmcblk1boot0 bs=512 seek=138
    echo 1 > /sys/block/mmcblk1boot0/force_ro
    mmc bootpart enable 1 1 /dev/mmcblk1

    # My emmc has an 8g user area and two 16MiB boot partitions.
    # I've tried zeroing them all out and applying SPL to one
    # at a time to verify I am programming/using the correct area
    # of flash. Everything appears ok, and I am able to boot my
    # 2015 version of u-boot from emmc using the same steps.

b) checking the extcsd info on the emmc to make sure boot
   partition is enabled. Also played around with Boot bus conditions
   but wound up leaving them at 0x0.
    
    Boot configuration bytes [PARTITION_CONFIG: 0x48]
     Boot Partition 1 enabled                                             
     No access to boot partition             

    Boot bus Conditions [BOOT_BUS_CONDITIONS: 0x00]         

    # I've tried all combinations I could find, none worked better,
    # many worked worse.

c) after POR, checking smbr1/sbmr2 (they look mostly ok)
    sbmr1=10004860   

            [cfg4: 10 - ECSPIx_SS1 - pulled high by mistake,
                             shouldn't hurt?]
            [cfg3: 00 - reserved]
            [cfg2: 48 - 8-bit, eSDHC2, 0-500/400mhz, 3.3v]
            [cfg1: 60 - emmc, regular-boot, high-speed,
                    fast-boot-ack-enb,
                    no-sd-power-cyc, thru-sd]

    sbmr2=02000041    [bmod=internal, 4=??, sec_config=open]

d) after POR, checking whether ivt got loaded in ocram (it did).
        J-Link>mem32 907400,c
        00907400 = 402000D1 00908000 00000000 00000000
        00907410 = 00907420 00907400 00000000 00000000
        00907420 = 00907000 0000D000 00000000 400400D2

e) checked SPL ivt header for correctness
   (script from https://community.nxp.com/docs/DOC-102453)

    $ python3 imxbin.py SPL
    =================IVT data===================
    ivt_length=20
    ivt_entry=908000
    ivt_dcd=0
    ivt_boot_data=907420
    ivt_self=907400
    ivt_csf=0
    =================DCD data===================
    No DCD data in table

f) after POR, checking whether code got loaded into ocram (usually not!)
    Why is ivt okay but this never loaded or overwritten?
    J-Link>mem32 908000,8
    00908000 = 5880BCE7 9EB3322F E4B82B75 BCA61DFB
    00908010 = D81D695D 59B3F13D 483D24F5 21F92F47

    when loading from usb-sdp this contains correct spl code, and it
    stays there all the way thru the main u-boot prompt. why different?
    J-Link>mem32 908000,8
    00908000 = EA00000F E59FF014 E59FF014 E59FF014
    00908010 = E59FF014 E59FF014 E59FF014 E59FF014

Any other ideas on how to debug this? It seems like (f) is a big clue, but
I don't know where to go with it. Hopefully something simple!

Labels (3)
0 Kudos
Reply
1 Reply

1,431 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robert

one can look on spl tutorial on

ventana/bootloader – Gateworks 

NXP does not support i.MX6 uboot spl in its official software,

issue may be posted on uboot mailing list

U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply