Trigger DMA when a GPIO signal is high i.MX RT1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Trigger DMA when a GPIO signal is high i.MX RT1170

跳至解决方案
621 次查看
Haitham_Ismail
Contributor III

I am using lpspi edma sdk to transfer data between i.MX RT1170 board (master) and a slave device. I was successful in sending the commands from the master. What I want now is to trigger DMA Rx on the master when the slave sends a high signal on a GPIO connection between the two devices. How I can set that up?

iMXRT1170 

0 项奖励
回复
1 解答
585 次查看
jingpan
NXP TechSupport
NXP TechSupport
0 项奖励
回复
1 回复
586 次查看
jingpan
NXP TechSupport
NXP TechSupport
0 项奖励
回复