Trigger DMA when a GPIO signal is high i.MX RT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Trigger DMA when a GPIO signal is high i.MX RT1170

Jump to solution
461 Views
Haitham_Ismail
Contributor III

I am using lpspi edma sdk to transfer data between i.MX RT1170 board (master) and a slave device. I was successful in sending the commands from the master. What I want now is to trigger DMA Rx on the master when the slave sends a high signal on a GPIO connection between the two devices. How I can set that up?

iMXRT1170 

0 Kudos
1 Solution
1 Reply
426 Views
jingpan
NXP TechSupport
NXP TechSupport
0 Kudos