How to trigger a LPSPI3 DMA transfer from a GPIO dropping edge

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to trigger a LPSPI3 DMA transfer from a GPIO dropping edge

Jump to solution
566 Views
tbiberdorf
Contributor IV


I want to trigger a 25 byte DMA data transfer on the LPSPI3 being triggered by a dropping edge GPIO input.

I am using: MCUXpresso IDE v11.4.1 [Build 6260] [2021-09-15] toolchain

and working on a IMXRT1060 EVKB development board. (note I did add the needed resistors to support the Arduino pin connections (J17-4, J17-5 & J17-6)

I have mapped the LPSPI3 pins:
* MOSI J23-23
* MISO J23-7
* CLK J23-21
* CS J23-22

I have a signal generator sending a 3.3V square wave pulse to the Arduino pin: J17-6 GPIO_SD_B0_00
(which is configured to use XBAR1_INOUT4)

To confirm that my signal is present I'm mirroring this signal to Arduino pin: J17-5 GPIO_SD_B0_03
(which is configured to use XBAR1_INOUT6)

I have my XBAR output 3 to start DMA channel 8 to set/clear GPIO pin: J17-4 GPIO_SD_B0_02

Channel 8 that is performing the set/clear operations on GPIO_SD_B0_02 is also chained to start the LPSPI3 data transfer, which in turn is changed to a channel 7 to set the GPIO pin.

The sample code can be found and loaded from the following GitHub repo branch develop: https://github.com/tsbiberdorf/SPI3-DMA-FromGPIO.git

The sample code is run by entering a character into the UART port on the EVKB board.

This test can be run by issuing the character '6'. Other tests are made available in this sample code, please read the description if you want to run them, but my concern here is for test '6'.

In this test, I am configured XBAR1 to receive my dropping edge GPIO signal (P17-6). The XBAR1 will then output a DMA operation on XBAR1_INOUT3 to start the DMA0 channel 8.

DMA0-ch8 will clear P17-4 then it should start DMA0-ch6 to execute a 25 byte DMA operation from LPSPI3 peripheral. When this transfer is completed, it will then activate DMA0-ch7 to set pin P17-4.

DMA0-ch5 has been configured to read all data received from LPSPI3 bus. it will also call for a IRQ complete when completed.

DMA0-ch7 will be called to set the Arduino pin P17-4 to signal that the data transfer has been completed.

A major problem that I cannot figure out is why does a part of the SPI3 transfer happen at the start of my test '6', and then when the dma ch8 is completed does it not start again? My guess is that the SPI3 peripheral is locked up, but I'm not sure why or how to fix it.

Can someone please help explain what I am doing wrong?

Thanks

 

This is what a logic analyzer capture of the listed pins indicates:

tbiberdorf_0-1675455995507.png

so you can see that when command '6' is issued, the XBAR triggers J15-5 to clear and the SPI transfer starts, but does not complete all 25 bytes.  it appears that 25 dropping edges of J17-6 is measured (by the mirror on J17-4) till the dma channel 7 is started to set J17-5.

After this first cycle, no further SPI 3 traffic is measured, but the the number of dropping edges does match the number of bytes that should be transferred.

 

0 Kudos
1 Solution
507 Views
tbiberdorf
Contributor IV

I found the solution.  I created test case '8', '9', & 'a' to demonstrate the configuration and operations.

 

View solution in original post

0 Kudos
4 Replies
514 Views
tbiberdorf
Contributor IV

source code is now attached.

0 Kudos
563 Views
tbiberdorf
Contributor IV

To show results that I measure when I test command '5':

I can see J17-5 does clear then set again on each dropping edge of J17-6:

tbiberdorf_0-1675456361200.png

zoom in on one of the transfers:

tbiberdorf_1-1675456402380.png

So I am confident that the XBAR triggering the GPIO pins changing states does work.

0 Kudos
560 Views
tbiberdorf
Contributor IV

Test command '4' was made to prove that the SPI DMA transfer could be setup once and then just started using the commands:

dmaBASE->SERQ = DMA_SERQ_SERQ(0); // eDMA starts transfer RX channel
dmaBASE->SERQ = DMA_SERQ_SERQ(1); // eDMA starts transfer TX channel

tbiberdorf_0-1675456575753.png

 

This was used as a basis to apply to the multi chain operation after the GPIO dropping edge is first detected.

0 Kudos
508 Views
tbiberdorf
Contributor IV

I found the solution.  I created test case '8', '9', & 'a' to demonstrate the configuration and operations.

 

0 Kudos