I am trying to train a face detection model using the eIQ portal. I am trying to import dataset from tensorflow dataset (tfds) specifically coco/2017 dataset. However, I only want to import wider_face. But when I try to do that, Importer error occurs which is shown in the image below. Any help will do. Thanks!
Also, the link you provide is already a pre-trained model. I am trying to train my model from the scratch by importing from tensorflow datasets using the eIQ portal.
But it seems that there are errors downloading the dataset.
I already have do that process before but Im referring to the wider_face dataset from tfds since I only wanted to focus on face detection.
Steps are:
1. Import dataset
2. Select tensorflow datasets
3. Select object detection
4. Go to advance options and choose wider_face dataset
5. Split dataset to 80%/20%
The error happens from step 1. I tried to download the whole coco2017 dataset aswell but I just want to use the face detection instead thats why I select wider_face dataset.