Hello,
we are currently planning a real time application which should executed on the Cortex-M4 of the i.MX8 platform during a performance intensive application is running on the Cortex-A35.
The Cortex-M4 application communicates with SPI/I2C hardware interface
The Cortex-A35 application displays information on the GUI
Therefore we have compared the following i.MX8 platform datasheets:
After comparing the system block diagram between the IMX8MPRM and IMX8DQXPRM platforms,
the following questions have arisen:
Thank you for your answer in advance.
Best regards,
David
IMX8DQXPRM Block Diagram:
IMX8MPRM Block Diagram:
解決済! 解決策の投稿を見る。
Hi David
>Do both SoCs use the same bus system architecture?
no
>The IMX8MPRM manual describes an AXI and AHB Switch Fabric
>The IMX8DQXPRM manual just mension a SSI (Source Synchronous Interface)-Interface between the >subsystems on the platform
>What is the difference between SSI system bus and the AXI and AHB Switch Fabric?
additional info was sent via mail.
>All communications to subsystems such as offchip memory or SPI run via the system bus (the bottleneck).
>Is it still possible to access the SPI/I2C by the Cortex-M4 in hard real time via the system bus?
yes
>Is there already a newer revision of the i.MX8X platform manual IMX8DQXPRM?
latest on official web product page
Best regards
igor
Hi David
>Do both SoCs use the same bus system architecture?
no
>The IMX8MPRM manual describes an AXI and AHB Switch Fabric
>The IMX8DQXPRM manual just mension a SSI (Source Synchronous Interface)-Interface between the >subsystems on the platform
>What is the difference between SSI system bus and the AXI and AHB Switch Fabric?
additional info was sent via mail.
>All communications to subsystems such as offchip memory or SPI run via the system bus (the bottleneck).
>Is it still possible to access the SPI/I2C by the Cortex-M4 in hard real time via the system bus?
yes
>Is there already a newer revision of the i.MX8X platform manual IMX8DQXPRM?
latest on official web product page
Best regards
igor
Hello,
Can you clarify more about
What is the difference between SSI system bus and the AXI and AHB Switch Fabric?
Chenjin