Hello,
I am trying to display a splash screen at u-boot.
I have been following the instructions in the i.MX_Reference_Manual_Linux.pdf (IMXLXRM Rev.L4.9.88_2.0.0-ga, 05/2018), 6.2.6.1.2.7 Enabling an EPDC Splash Screen:
- updated mx6sllevk.h (added the 2 defines) and re-compiled, regenerated the image (DISTRO='fsl-imx-fb' MACHINE=imx6sllevk source fsl-setup-release.sh)
- converted the EPD060XH2C1.fw into epdc_splash.bin
- copied the epdc_splash.bin into the FAT partition
At reboot, I still do not see a splash screen.
Is there a default splash screen that should be displayed? Where do I modify the source of the default splash screen or logo?
Solved! Go to Solution.
I was finally able to display the splash screen.
All I had to do was:
1- adjust the local.conf and add UBOOT_CONFIG = "sd epdc"
2- Add epdc_splash.bin waveform file in boot partition
3- Add epdc_logo.pgm in boot partition
I was finally able to display the splash screen.
All I had to do was:
1- adjust the local.conf and add UBOOT_CONFIG = "sd epdc"
2- Add epdc_splash.bin waveform file in boot partition
3- Add epdc_logo.pgm in boot partition
Hello,
Does this guide also apply to EPDC?
Hello ekerebel,
You can follow the guide made by one of our third party:
https://developer.toradex.com/knowledge-base/u-boot-splash-screen
Regards
@Bio_TICFSL Does this guide also apply to EPDC?