Setting custom HDMI timing for i.MX8 Quad Max

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting custom HDMI timing for i.MX8 Quad Max

692 Views
yavuz_mutlu
Contributor II

Hi all,

 

We are trying to add support for non-standard HDMI display timings for our display. As far as I understand we need to add clock support for our DRM mode which is

{ DRM_MODE("4096x640", DRM_MODE_TYPE_DRIVER, 175560, 4096, 4144,
4188, 4290, 0, 640, 672, 674, 682, 0,
DRM_MODE_FLAG_PHSYNC | DRM_MODE_FLAG_NVSYNC),
.vrefresh = 60, },

 

I don't think i.MX 8 QM with 5.4.70 kernel supports 175560 clock frequency. In some other questions people mentioned and added some patches to support their timings, however, I think HDMI driver structure has completely changed for this kernel (and the documentation https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf seems to be wrong).

 

How to add custom clock support for our timings?

Thanks in advance.

 

0 Kudos
Reply
1 Reply

643 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

The first thing would be to check if that specific frequency can be achieved by some of the available clock sources. For the latest Linux docs (L5.4.70_2.3.1_LINUX_DOCS), you may refer to the following link in which in table 5 you will find the link for the i.MX Graphics DRM's repo: https://www.nxp.com/webapp/Download?colCode=L5.4.70_2.3.1_LINUX_DOCS 

 

Hope it helps!

 

BR,

Ivan.

0 Kudos
Reply