Setting IMx8MQ Mipi CSI2 clock for OV5640 RAW8 BIT Bayer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting IMx8MQ Mipi CSI2 clock for OV5640 RAW8 BIT Bayer

3,515 Views
jhpark_vine
Contributor III

ov5640_clock.PNG

 

1.  From above OV5640 Clock pipeline,    we'd like to change  MIPISCLK - 672 MHz to 456 MHz ,

  then How to setup MIPI CSI2 DPhy  Clcok ?

 

  Below is for i.MX6 MPU ,  how to setup DPHY Clock for  i.Mx8M Quad? 

  do we modify mipi_csi_1: mipi_csi1@30a70000  device tree ? 

 from   https://www.nxp.com/docs/en/application-note/AN5305.pdf 

MIPI D-PHY Clock for i.MX6  MPU.

3.4. MIPI D-PHY clock
The camera sensor (the sensor output differential clock) drives and controls the MIPI D-PHY clock.
The MIPI D-PHY clock must be calibrated to the actual clock range of the camera sensor’s D-PHY
clock and the calibrated value must be equal to or greater than the camera sensor clock. This frequency
ranges from 80 MHz to 1000 MHz.
The MIPI D-PHY clock must be set according to a known value of the camera sensor’s pixel clock. This
must be a known value or a value measured with an oscilloscope during a high-speed burst.
To calculate the MIPI data rate, use these equations:
MIPI data rate = (MIPI clock * 2) * Number of lanes >= Pixel clock * Bits-per-pixel
MIPI clock = (Pixel clock * Bits-per-pixel) / (Number of lanes) / 2
For example, a video input of 720p, 59.94 fps, and YUV422 is calculated as follows:
Pixel clock = 1280 * 720 * 59.94 fps * 1 cycle/pixel * 1.35 blank interval = 74.57 MHz
Total MIPI data rate is 74.25 M * 16 bits = 1193 Mb/s.
The frame blank intervals and the interface packaging overhead were added as the 1.35 factor in the
pixel clock equation above.
For a 2-lane interface:
MIPI clock = 1193 / 2 / 2 = 298.25 MHz
MIPI_CSI2_PHY_TST_CTRL1 setting = 298.25 MHz * 2 (DDR mode) = 596.5 MHz
According to Table 2, MIPI_CSI2_PHY_TST_CTRL1 = 0x2E.
For a 4-lane interface:
MIPI clock = 1193 / 4 / 2 = 149.12 MHz
MIPI_CSI2_PHY_TST_CTRL1 setting = 149.12 MHz * 2 (DDR mode) = 298.24 MHz
According to Table 2, MIPI_CSI2_PHY_TST_CTRL1 = 0x28.

 

-- device tree file --

mipi_csi_1: mipi_csi1@30a70000 {
compatible = "fsl,mxc-mipi-csi2_yav";
reg = <0x30a70000 0x1000>;
interrupts = <GIC_SPI 44 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_CSI1_CORE>,
<&clk IMX8MQ_CLK_CSI1_ESC>,
<&clk IMX8MQ_CLK_CSI1_PHY_REF>;
clock-names = "clk_core", "clk_esc", "clk_pxl";
assigned-clocks = <&clk IMX8MQ_CLK_CSI1_CORE>,
<&clk IMX8MQ_CLK_CSI1_PHY_REF>,
<&clk IMX8MQ_CLK_CSI1_ESC>;
#ifndef PIXEL_RAW
assigned-clock-rates = <133000000>, <100000000>, <66000000>;
#else
assigned-clock-rates = <266000000>, <150000000>, <66000000>;
#endif
/*
assigned-clock-parents = <&clk IMX8MQ_SYS1_PLL_266M>,
<&clk IMX8MQ_SYS2_PLL_1000M>,
<&clk IMX8MQ_SYS1_PLL_800M>;
*/
power-domains = <&pgc_mipi_csi1>;
csis-phy-reset = <&src 0x4c 7>;
phy-gpr = <&iomuxc_gpr 0x88>;
status = "disabled";
};

csi1_bridge: csi1_bridge@30a90000 {
compatible = "fsl,imx8mq-csi", "fsl,imx6s-csi";
reg = <0x30a90000 0x10000>;
interrupts = <GIC_SPI 42 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_CSI1_ROOT>,
<&clk IMX8MQ_CLK_DUMMY>;
clock-names = "disp-axi", "csi_mclk", "disp_dcic";
status = "disabled";
};

 

2. what is link-frequency from above picture ?

  is it a  MIPI_CLK or MIPISCLK? 

 

3.  To set  link frequency other  MHZ ( ex, 300Mhz ) , then how should we modify  MIPI CSI2 host Controller -  mxc-mipi-csi2_yav.c ?

static void mxc_mipi_csi2_hc_config(struct mxc_mipi_csi2_dev *csi2dev)
{
u32 val0, val1;
u32 i;

val0 = 0;

/* Lanes */
writel(csi2dev->num_lanes - 1,
csi2dev->base_regs + CSI2RX_CFG_NUM_LANES);

for (i = 0; i < csi2dev->num_lanes; i++)
val0 |= (1 << (csi2dev->data_lanes[i] - 1));

val1 = 0xF & ~val0;
writel(val1, csi2dev->base_regs + CSI2RX_CFG_DISABLE_DATA_LANES);

/* Mask interrupt */
writel(0x1FF, csi2dev->base_regs + CSI2RX_IRQ_MASK);

writel(1, csi2dev->base_regs + 0x180);
/* vid_vc */
writel(1, csi2dev->base_regs + 0x184);
writel(csi2dev->send_level, csi2dev->base_regs + 0x188);
}

static int mipi_csi2_clk_init(struct mxc_mipi_csi2_dev *csi2dev)
{
struct device *dev = &csi2dev->pdev->dev;

csi2dev->clk_core = devm_clk_get(dev, "clk_core");
if (IS_ERR(csi2dev->clk_core)) {
dev_err(dev, "failed to get csi core clk\n");
return PTR_ERR(csi2dev->clk_core);
}

csi2dev->clk_esc = devm_clk_get(dev, "clk_esc");
if (IS_ERR(csi2dev->clk_esc)) {
dev_err(dev, "failed to get csi esc clk\n");
return PTR_ERR(csi2dev->clk_esc);
}

csi2dev->clk_pxl = devm_clk_get(dev, "clk_pxl");
if (IS_ERR(csi2dev->clk_pxl)) {
dev_err(dev, "failed to get csi pixel link clk\n");
return PTR_ERR(csi2dev->clk_pxl);
}

return 0;
}

 

PHY_GPR.PNG

 

 

  can you inform me DPHY Register setting  on IMX8M Quad ?

  do we modify  mipi_csi_1 clock setting  from  above mx8mq device tree ?

  assigned-clock-rates = <133000000>, <100000000>, <66000000>; 

4.  finally, if we'd like to Raw8 bit from OV5640 ,  then should we modify  capture driver   - ov5640_mipi_v2.c ? 

    It seems to support  RAW8Bit  Bayer  ( SBGGR8)  by default .

     cant you inform me how to setup  CSICR1, CSICR2, CSICR3,  CSI_CSIIMAG_PARA , CSICR18  registers ? 

 

5.  For CSICR2 setting,  can you inform me how to set  BTS (Bayer tile Start)  at  5005 page from Reference manual ? 

 

BTS.PNG

 

6. For CSICR18 setting , how to setup Mask_option ( 19-18 Bits )  at 5019 page from Reference Manual ? 

MASK.PNG

Thanks . 

  

    

  

 

 

 

 

 

0 Kudos
Reply
2 Replies

3,501 Views
igorpadykov
NXP Employee
NXP Employee

Hi JungHwan

 

for raw8 one can look at example below

https://community.nxp.com/t5/i-MX-Processors/iMX8M-MIPI-CSI-4-lane-configuration/m-p/875755

 

Best regards
igor

0 Kudos
Reply

3,487 Views
jhpark_vine
Contributor III

Link Frequency is  MIPI Clock from Tovalds. 

/* Calculate the line rate from the pixel rate. */

link_freq v4l2_get_link_freq(state->src_sd->ctrl_handler, state->csi2_fmt->width, state->bus.num_data_lanes * 2);

 

s64 v4l2_get_link_freq(struct v4l2_ctrl_handler *handler, unsigned int mul,
unsigned int div)
{
struct v4l2_ctrl *ctrl;
s64 freq;

ctrl = v4l2_ctrl_find(handler, V4L2_CID_LINK_FREQ);
if (ctrl) {
struct v4l2_querymenu qm = { .id = V4L2_CID_LINK_FREQ };
int ret;

qm.index = v4l2_ctrl_g_ctrl(ctrl);

ret = v4l2_querymenu(handler, &qm);
if (ret)
return -ENOENT;

freq = qm.value;
} else {
if (!mul || !div)
return -ENOENT;

ctrl = v4l2_ctrl_find(handler, V4L2_CID_PIXEL_RATE);
if (!ctrl)
return -ENOENT;

freq = div_u64(v4l2_ctrl_g_ctrl_int64(ctrl) * mul, div);

pr_warn("%s: Link frequency estimated using pixel rate: result might be inaccurate\n",
__func__);
pr_warn("%s: Consider implementing support for V4L2_CID_LINK_FREQ in the transmitter driver\n",
__func__);
}

return freq > 0 ? freq : -EINVAL;
}

 

Then how do we set  MIPI D-PHY Clock ? 

 

0 Kudos
Reply