With respect to the SABRE platform's Audio interface, "Serial over Audio IN/Audio OUT support" is possible through the Audio Jack?
Can this feature be implemented only through software or are any hardware changes required ?
已解决! 转到解答。
Hi Pankaj
yes this may be performed using telephony modem algorithms.
Very simply put, for example using amplitude modulation:
Snd 1000KHz sinusoid with amplitude "0" - means digital "0".
Send 1000KHz sinusoid with max. amplitude "0xff" - means digital "1".
On receiving side one needs to decode it in software.
Other more complicated methods FM modulations (such as 2400Hz - "1",
1200Hz - "0") one can read in V22 and other telephony modem specs.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pankaj
yes this may be performed using telephony modem algorithms.
Very simply put, for example using amplitude modulation:
Snd 1000KHz sinusoid with amplitude "0" - means digital "0".
Send 1000KHz sinusoid with max. amplitude "0xff" - means digital "1".
On receiving side one needs to decode it in software.
Other more complicated methods FM modulations (such as 2400Hz - "1",
1200Hz - "0") one can read in V22 and other telephony modem specs.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------