Sample source of DDR bus clock change

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sample source of DDR bus clock change

Jump to solution
1,664 Views
ko-hey
Senior Contributor II

Hi all

I'm using i.MX6SL with Linux Yocto and want to change DDR3's bus clock for sysytem evalutation.

I found some sources in BSP such as busfreq-imx6.c、busfreq-ddr3.c and busfreq-lpddr2.c.

However, I think those files are for i.MX6Q/D/DL/SL.

Does anyone have a sample source for i.MX6SL ?

If anyone doesn't have sample source, please teach me where I should change.

Ko-hey

Labels (3)
0 Kudos
Reply
1 Solution
1,402 Views
joanxie
NXP TechSupport
NXP TechSupport

one can try to refer to the patch for L3.0.35

<i.MX6SL DDR3 support for L3.0.35_2.1.0 >.

View solution in original post

0 Kudos
Reply
2 Replies
1,403 Views
joanxie
NXP TechSupport
NXP TechSupport

one can try to refer to the patch for L3.0.35

<i.MX6SL DDR3 support for L3.0.35_2.1.0 >.

0 Kudos
Reply
1,402 Views
ko-hey
Senior Contributor II

Hi Guanqiong Xie

Thanks.

I'll try it.

Ko-hey

0 Kudos
Reply