SRKH register key values for i.MX6 & i.MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRKH register key values for i.MX6 & i.MX8

889 Views
jbhaijy
Contributor III

Dear Experts,

We have SRKH register key values setup for i.MX6. Now we are migrating from i.MX6 to i.MX8, so can we use the same values that we use for the i.MX6?

 

Regards,

Yunus

0 Kudos
Reply
4 Replies

870 Views
jbhaijy
Contributor III

Any update on above query?

0 Kudos
Reply

866 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @jbhaijy 

I hope you are doing well
 
can we use the same values that we use for the i.MX6?
=> No, We will recommend you to use the new value for that board.
 
Thanks & Regards
Sanket Parekh
0 Kudos
Reply

861 Views
jbhaijy
Contributor III

Hi Sanket, 

Thanks for response.

May I know the reason why we cannot use the same SRKH key value for i.MX8? Is there any SoC specific reason? Please provide some more info. 

0 Kudos
Reply

842 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @jbhaijy 

I hope you are doing well.
 
As both the boards have many architecture wise differences and NXP can not recommend with the same efuses as it is one time programmable. 
One can refer to the section . 1.7 Programming SRK Hash of document root/doc/imx/habv4/guides/mx8m_mx8mm_secure_boot.txt
 
"Be careful when programming these values, as this data is the basis for the root of trust. An error in SRK Hash results in a part that does not boot."
 
Thanks & Regards
Sanket Parekh
0 Kudos
Reply