Flashing android 12.1.0 on sd card for imx8qxp failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing android 12.1.0 on sd card for imx8qxp failed

2,483 Views
vsuneja63
Contributor III

Hi,

Thanks!

I could build android 12.1.0 for imx8qxp-mek target & trying to flash sd card for the same. Inserted sd card in the board & change settings to download mode.
I used uuu tool to flash in sd card but it's always failing with 'partition doesn't exist' error. Below are the logs:

agl@agl-OptiPlex-7010:~/AAos/NXP-imx8/Android_Auto12/android_build/out/target/product/mek_8q$ sudo ./uuu_imx_android_flash.sh -f imx8qxp -a -e -u c0 -c 28 -t sd_all
This script is validated with uuu 1.4.182 version, it is recommended to align with this version.
dual bootloader is supported
dtbo is supported
dual slot is supported
has system_ext partition
generate lines to flash spl-imx8qxp-c0.bin to the partition of bootloader0
generate lines to flash partition-table-28GB.img to the partition of gpt
generate lines to flash bootloader-imx8qxp-c0.img to the partition of bootloader_a
generate lines to flash dtbo-imx8qxp.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash system_ext.img to the partition of system_ext_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash product.img to the partition of product_a
generate lines to flash vbmeta-imx8qxp.img to the partition of vbmeta_a
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.182-0-ga561ed7

Success 0 Failure 1


1:14 7/21 [partition does not exist ] FB[-t 600000]: flash bootloader_a bootloader-imx8qxp-c0.img

Any suggestion on this could be really helpful. Looking forward for your response.

0 Kudos
Reply
3 Replies

2,434 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @vsuneja63 

1.Please share your SD card size

2.Try to flash emmc

3.Have you tried the demo image?

0 Kudos
Reply

2,407 Views
vsuneja63
Contributor III

Hi,

Thanks!

I could flash emmc via uuu tool but my requirement is to go with sd card. I am using sd card of 32GB.

I have not tried demo image yet.

0 Kudos
Reply

2,448 Views
vsuneja63
Contributor III

Hi,

Thanks!

Any suggestion on this issue?

0 Kudos
Reply