SAIF2 interrupt on iMX233 (WINCE6 R3)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SAIF2 interrupt on iMX233 (WINCE6 R3)

528 次查看
MenM
Contributor I

Hi,

I try to get SAIF2 up and running on a iMX233. I see that the DMA command complete interrupt is set after a DMA transfer, but my thread is not serviced. If I do the same with SAIF1 everything works fine. (SAIF1is using another interrupt number)

anyone ho has ever tried using SAIF2 on an iMX233 or any suggestions to debug the interrupt piece from dma to interrupt controller?

thanks in advance,

Maarten.

标记 (1)
0 项奖励
回复
0 回复数