SAI3 port data line's pull select fields

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SAI3 port data line's pull select fields

655件の閲覧回数
ganapathiraopil
Contributor I

Hi,

I am trying to add a new sound card as an external mic to record the voice in imx7d board, for this I am configuring sai3 port. For sai3 , the available pull select fields are 100K PD, 5K PU, 47K PU and 100K PU. So on which basis we need to select these values. Do we have any proper format to follow while configuring these pull fields or we can have any of these available values?.

Kernel version - 4.1.15

Please help me regarding this.

Thanks in advance.

Regards,

Ganapathirao

ラベル(1)
0 件の賞賛
返信
1 返信

578件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ganapathirao

some signals may be tristated (both codec and i.MX7) as described in

Table 13-44. SAI External Signals i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

so pad settings should be set appropriately. Settings provided in NXP

software : linux and FreeRTOS bsps can be used as starting point

and adjusted based on waveforms required by datasheet.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信