Hello All,
Need some infomation regarding SABRE for Automotive
Infotainment Based on the i.MX 6 Series: uuu flashing.
I have the following board IMX6SABREINFOQSG.pdf .I need to boot from MMC (no sd card). I have made the switch as mentioned in the document. Devices goes to recovery mode also and uuu script is used to flash. Serial console is opened, so while running the uboot log should come right, it is not coming. UUU script is also stuck (1/2).
does /IMX6SABREINFOQSG has on board mmc...? How to proceed forward
Note:
Used yocto to make , machine name= imx6qsabresd
UUU commands
sudo uuu -v u-boot-imx6qsabresd.imx
sudo uuu -d u-boot-imx6qsabresd.imx
With these command i am expecting u-boot log in the UART debug port.
Linux BSP version you have built using Yocto?
linux-imx : 5.15.32
DISTRO command used
DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd source imx-setup-release.sh -b build
Please see the below switch mode, i have selected MMC flash/boot
Boot mode switch value:
S2
S2:1= OFF | S2:2 = ON | S2:3 = ON | S2:4 = OFF |
S1
S1:1 = OFF | S1:2 = ON | S1:3 = OFF | S1:4 = OFF | S1:5 = ON | S1:6 = ON | S1:7 = OFF | S1:8 = OFF | S1:9 =OFF | S1:10 =OFF |
S3
S3:1 = OFF | S3:2 = ON | S3:3 = OFF | S3:4 = ON |
Hi,
Thank you for providing such detailed information.
From this, I see that you have built using the i.MX6Q Sabre as MACHINE, this will create all files for the SABRESD board, this image will not boot on sabre automotive.
Unfortunately i.MX6 sabre automotive has been dropped from Yocto due to end of life, so it is not possible to select the imx6qsabreauto machine to build it.
It may be possible to build using standalone method as specified in the i.MX Poting Guide
https://www.nxp.com/docs/en/user-guide/IMX_PORTING_GUIDE.pdf
Also, for a quick start you may try with last released pre-built image (L5.10.72_2.2.2)
https://www.nxp.com/webapp/Download?colCode=L5.10.72_2.2.2_MX6QDLSOLOX&appType=license
Best regards,
Aldo.