change Imx287 power prep settings in yocto project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

change Imx287 power prep settings in yocto project

Jump to solution
1,319 Views
ireshj
Contributor II

hi,

 

I m developing a yocto-based (kirkstone) os for a custom board with im287 chip. currently, I have a working image for imx28evk board, now i need to port it to the custom board.

there I m facing an issue with changing the power prep settings as the custom board should not check on the battery voltage, but the uboot for the imx28evk falls to start as there's no battery in the custom board.

I went through imx porting guide and imx yocto projects user guide but could not figure out where to apply the power prep settings

much appreciated if anyone can point where to look

Labels (2)
0 Kudos
Reply
1 Solution
1,314 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello ireshj,

Sorry, NXP does not have continues with yocto on MX28 since kernel 3.10, and now you are in kirkstone you have to go with community BSP:

https://www.yoctoproject.org/community/

 

Regards

 

View solution in original post

0 Kudos
Reply
1 Reply
1,315 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello ireshj,

Sorry, NXP does not have continues with yocto on MX28 since kernel 3.10, and now you are in kirkstone you have to go with community BSP:

https://www.yoctoproject.org/community/

 

Regards

 

0 Kudos
Reply