Dear All,
i.MX6 DDR Stress Test Tool V1.0.3
I need to get some information regarding DDR ram calibration and memory stress test for new layout related to iMAX6 Quad hardware design. In my custom design I have included only USB port & SD card slot.
To do stress test for RAM do we need to use SATA HDD ? Can't we use good SD card for that. Or else can I use portable HDD connecting via USB for this ? (I don't have SATA port in my custom hardware design)
I'm referring to following test >> http://www.imx6rex.com/software/stress-testing-stressapptest/#test_mem
What is the difference between the test you have provided here >> https://community.nxp.com/docs/DOC-105652 and above mentioned test ? Do we need SATA HDD for this stress test too ?
I must be thankful to you if you will kindly reply me soon.
Regards,
Peter.
Solved! Go to Solution.
Hi Peter
nxp developed i.MX6 DDR Stress Test Tool V1.0.3 ddr test tool,
it does not use sata or sd. Other tools, like mentioned above developed by
third parties and questions may be posted to developers of those tools.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thank you very much for the quick response.
I'm trying to do stress test and RAM calibration for imx6q sbre sdb development board using i.MAX6 DDR Stress test tool V2.60 >> https://community.nxp.com/docs/DOC-105652 <<
When I go through the above link I couldn't understand how should I approach for this as I'm new to this test. So could you please provide me well detailed document for this.
**********************************************************************
>> Option 1 GUI based:
Run the GUI executable and connect your board to the host PC via USB
***********************************************************************
I must be thankful to you if you will kindly reply me soon.
Regards,
Peter.
1. DDR_Tester.exe
2. OTG
3. PC
4. PC
Best regards
igor