From i.MX 6Solo/6DualLite Applications Processor Reference Manual, Rev. 4, 07/2018
38.1.2.1.6.1 Screen Refresh
• The refresh rate may vary within a predefined range. Within this range, the rate is
dynamically adjusted to the content update rate.
• An indication about the availability of new content is obtained as follows:• If the page-flip double buffering is used, the mechanism provides this indication
• If only a single buffer is used (and incrementally updated), the IPU can receive
an indication of a modification from the ARM platform (by setting an internal
flag).
• The IPU counts the refresh cycles: the total and those with new content. The ARM
platform can use these counters to optimize display management (e.g. switching
display buffer compression on/off). The counters are reset by the ARM platform.
• The transferred data may be processed on the way, using the IC and DP.
IPU is counting display refresh cycles according to above description.
I would like to check this counter for debugging our system.
Could you please teach me register name to get the counted value?
Best Regards,
Kazuma Sasaki.
Solved! Go to Solution.
Hello Kazuma Sasaki,
I made some research and the counter for refresh cycles is not accessible as it is part of the DP (Display Processor) and there is not a register from where this value could be read.
My apologies for the inconvenience.
Regards,
Hello Kazuma Sasaki,
I made some research and the counter for refresh cycles is not accessible as it is part of the DP (Display Processor) and there is not a register from where this value could be read.
My apologies for the inconvenience.
Regards,
Hello gusarambula,
Okay, I got it. Thank you for your support.
Best Regards,
Kazuma Sasaki.