Reboot period control for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Reboot period control for i.MX6

跳至解决方案
571 次查看
torus1000
Contributor V


Hi,

I observed VDDs during reboot. Some of them looks not enough OFF time then restart supplying.

Is there any way to stretch OFF time in terms of safe reboot?

I think watchdog control this period.

Where can I find about this in the manual?

Can anyone help me?

BR

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
453 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

processor or pmic has not internal hardware ability to stretch OFF time,

it may be done by external circuit, for example increasing RC value

R19,C504 on Sabre schematic SPF-27392 p.21 or using other similar

external circuits for extending pulse, like one shot trigger.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
454 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

processor or pmic has not internal hardware ability to stretch OFF time,

it may be done by external circuit, for example increasing RC value

R19,C504 on Sabre schematic SPF-27392 p.21 or using other similar

external circuits for extending pulse, like one shot trigger.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复