Reboot period control for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reboot period control for i.MX6

Jump to solution
569 Views
torus1000
Contributor V


Hi,

I observed VDDs during reboot. Some of them looks not enough OFF time then restart supplying.

Is there any way to stretch OFF time in terms of safe reboot?

I think watchdog control this period.

Where can I find about this in the manual?

Can anyone help me?

BR

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
451 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

processor or pmic has not internal hardware ability to stretch OFF time,

it may be done by external circuit, for example increasing RC value

R19,C504 on Sabre schematic SPF-27392 p.21 or using other similar

external circuits for extending pulse, like one shot trigger.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
452 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

processor or pmic has not internal hardware ability to stretch OFF time,

it may be done by external circuit, for example increasing RC value

R19,C504 on Sabre schematic SPF-27392 p.21 or using other similar

external circuits for extending pulse, like one shot trigger.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply