Read particular register through BLHOST in i.MXRT116x evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read particular register through BLHOST in i.MXRT116x evk

Jump to solution
544 Views
vishnusudhankj
Contributor III

HI,

Is it possible to read particular register through blhost (eg: 0x40c00000/0x400ec000)?

I can be able to read the flash memory location like 0x30002000. like is it possible to read particular arbitrary registers?

suggest steps to read the particular memory / registers through BLHOST?

0 Kudos
Reply
1 Solution
534 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @vishnusudhankj ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to read particular arbitrary registers?
-- No, I'm afraid not, to do that, you should use the debug tool.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
535 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @vishnusudhankj ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to read particular arbitrary registers?
-- No, I'm afraid not, to do that, you should use the debug tool.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply