I am using the MIMXRT1170-EVK, featuring the IS25WP128-JBLE QSPI NOR Flash. I have set up the hello world code such that the code is run from internal RAM, freeing up the flash for use.
I want to be able to read from the flash memory and also write to it and i cant seem to find the correct drivers required for this board.
How would i go about implementing this and what drivers/ additional files do i need to do so?
已解决! 转到解答。
Hi,
I thought this was the answer and AN12108 would provide the solution i am looking for however upon reflection i think my case is slightly different.
The Documents provided show how to drop files onto the board as if a mass storage device to be run from flash, or to boot from flash. My current query involves using the 1176's internal ram to boot ( which i have done), allowing me to write into flash some data and also extract(read) it back.
Is there any way to do this?